This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5141QRGEVM: Abnormal output waveform at SW node

Part Number: LM5141QRGEVM


Test board: LM5141QRGEVM

Test condition: VOUT = 5 V, DEMB mode, Frequency = 2.2 MHz, others are default set

                           VIN = 12 V, IOUT = 1 A (Electronic load)

As the figure shows, I observed abnormal waveform under above test condition. There are wide and narrow pulses at SW node. It looks like sub-harmonic, but actually the duty ratio is below 0.5 (VIN=12V,VOUT=5V). Meanwhile, the switching frequency is only 1 MHz, not 2.2 MHz.

My questions are summarized as follows:

1. How does the wide and narrow pulses at the SW node happen?  How to avoid this phenomenon?

2. Why the switching frequency is not 2.2MHz?