Part Number: TPS61322
Other Parts Discussed in Thread: ADS1299
Hello,
I have designed the circuit and 2layer PCB below for charging and boosting the output of a LiPo battery from 3.7V to 5V.
I am using the TPS613222ADBVT chip to boost the LiPo output from 3.7V to 5V.
When the switch is set to boost mode (disconnecting charge circuitry), I am getting 5V at the output as expected.
However, the board gets very hot in less than a minute. The inductor in particular gets extremely hot.
Can someone please tell me if this is normal, or if there is something wrong with my circuit that is causing it?
Is there any method to dissipate some of this heat without enlarging the footprint of the PCB too much?
Would more vias to the ground plane on the bottom layer help?