We use supervisory ckt TPS3836J25DBVR. Datasheet says its ESD sensitive but does not specify level . We had it classified as a Class 1 which is typical for this type of device The parts came in specified as Class 0 which does not make sense. TI states to treat this part as an ESD sensitive device; therefore the ESD level is needed to properly handle the device. Class 0 devices require special handling.
QA/ Reliability should have ESD level of TPS3836.