Is there a way to read the learned Qmax "Qmax Cell 0" learned value without un-sealing the device and reading the value via direct flash access?
Maybe there is a better way to do this but I would like to periodically read and report the learned Qmax when running tests on my fixtures and seeing how much the Qmax is changing.
I could read Qmax Cell 0 via the flash access like I read the "design energy scale" but only if it's unsealed.
I didn't see and of the standard, extended or sub commands I could used to read the Qmax value but maybe I missed something.
The FCC (Full Charge Capacity) command 0x6/0x7 is close to what I am looking for and may be close enough. I'm not sure how the Qmax value differs from what is reported with the FCC though.
Thanks,
Doug