Other Parts Discussed in Thread: LM5176
Tool/software: WEBENCH® Design Tools
I used Webench to design a power supply based on LM5176-Q1.
The design parameters were:
Output voltage: 24V
Output current: 8A
Input voltage: 11-50V
Switching frequency: 600 kHz
I have tested the circuit with a 4A load, varying the input voltage between 15 and 36V.
The power supply appears to be working - with one exception. When the input voltage is close to 24V, something weird happens. Current draw increases by approximately 1A (regardless of the load) and the inductor starts emitting noises that I learned to associate with instability. The only component that appears to get warmer is the inductor.
Any idea what may be causing this behavior?
Thanks!
Bart