Other Parts Discussed in Thread: LM337
Hi,
I would like to supply ± 2.5 V from ± 12 V input as a power supply using LM317 and LM337 as pressure sensors.
Attach the wiring diagram.
Please let me know if there is something wrong with the usage.
In particular, the values of the adjustment resistors are given in the respective data sheets of the LM317 and LM337.
We use the recommended values listed, but should we use the same constants?
Also, if the rise of ± 12 V is simultaneous, is it OK to recognize that the rise of ± 2.5 V is also simultaneous?
regards.