Other Parts Discussed in Thread: BQ25173
We are currently testing a new battery charger design that is based on the BQ25713 EVM module. I've seen this a couple times now where the charger appears to be working fine and charges a battery and then suddenly stops working. When it stops working these are the symptoms:
- When I connect VBUS from a bench top powersupply to try and charge the battery I hear an audible noise from the inductor and no current is drawn from the supply even when setting the charge voltage and current levels.
- The ACOV bit is set in the Charge Status Register?? I've measured with a scope and don't see any over voltage on VBUS. Why is this bit being set?
- The VREG LDO is coming up but I can see a periodic voltage spike riding on top the 6V waveform (also a periodic oscillation on VBUS)
- If I remove the battery and power the load from VBUS the switcher comes up and supplies power to the load (about 0.5A) with VSYS at 9V.
This is a new design and we're seeing quite a bit of fallout with the battery charger IC (BQ25173) on this first prototype so I'd like to understand this failure and hopefully determine the root cause. Any ideas why the ACOV bit is set and the battery charger is not charging when a battery is present?
Thanks,
Dan C.