According to my calculations the device is going to get too hot in my application, I can't find a MOSFET with a lower Qg and I don't want to drop the switching frequency. Is there a diode protecting the regulator? Can I connect Vbp to an external 8V source to reduce the load on the chip at high input voltages or will this damage the TPS40170?