Other Parts Discussed in Thread: LM5164
Would this devide be able to operate continuosly at 120°C and additionally 140°C only for 120 hours?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The ambient temperature is going to reach 140 degrees C for 120 hours in total, the rest of the time the ambient temperature will be around 120 °C and the power consumption will be around 0.7W
Hello,
For both 120 and 140 degrees C:
Input voltage 24-64
Output voltage 12
Load current 0.7
Hello,
For both 120 and 140 degrees C:
Input voltage 24-64 V, and nominal 48 V
Output voltage 12 V
Load current 0.7 A