Part Number: BQ76930
Other Parts Discussed in Thread: BQ76920,
With the BQ76930 (same applies to BQ76920), is there a way to manually force a reset on the IC without I2C?
For example, during some system transient states (let's assume these are unavoidable), the BQ IC has observed to get in a hung state, such that the input voltages are correct (after transient settle time) but the I2C is non-responsive. From the master (MCU) perspective, the lines appear to be reading high (i.e. not being held low), and manual bit bang STOP (SCL high, SDA low-to-high transition) does not recover. Unfortunately, I have not put an o-scope on this to confirm.
Cutting input power on BATT pin does not appear to work, since power is being fed back through a diode on VC10 and probably internal protection diodes on VCx pins (using EVM standard 1K resistors for filter). Due to alternate power paths, shunting the BATT pin to GND for a short duration doesn't seem like a good idea; or is this okay? Another idea is if a reserved function is within NC pin on IC that can be used to create a reset event. The only way to restore operation to BQ IC, is to physically remove the battery pack connection. This is not an option for field deployment.
Perhaps another way to look at addressing this issue, is if the BQ supply voltages fall below POR. According to datasheet, in very loud formatting, a "full device reset must be initiated by powering down both intermediate voltages (BAT-VC5X) and (VC5X-VSS) below Vshut and rebooting by applying the appropriate VBOOT signal to the TS1 pin". I'd like to create this condition without having the physically disconnect the entire battery pack, or adding a large FET switch network across all pack row voltages going in to the IC. If the later is what it takes, is there a recommended circuit I can evaluate?
Any guidance would be great, thank you.