In the design tab of the fusion digital power designer, one should set each capacitor's value. For example, if the rail contains 10 capacitors, the position of feedback of voltage is between the first capacitor and second capacitor, should I ignore the other 9 capacitors and only enter the value of first capacitor?
If in my design the output of rail is filtered by pi filter, should I enter the value of inductance? If so how can I enter the value of inductance?