This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478Q-Q1: Automobile grade circuit devices heat up to 100 degrees Celsius, help find out why

Part Number: LM3478Q-Q1
Other Parts Discussed in Thread: LM3478

MOSFET is PD70N1053,Vin 6~16V,Vout  12V or 15V  ,Iout=1A。All the devices on the circuit have a serious fever, up to 150 degrees Celsius, and the devices with heat sinks up to 100 degrees Celsius. The following table is the test results, please help to analyze the reasons? What should PCB pay attention to?