One customer is evaluating UC2895, but IC temperature is increase about 70℃(Ta: 20℃ ⇒90℃).
Please let me know about two points below;
①How to calculate IC's power dissipation
②Idea for decrease temperature (= IC's power dissipation)
Are Vin or fsw decrease, good effect?
UC2895 condition and information are below;
・Vin: 24V, fsw: 100kHz, Duty: 50% (Push-Pull)
・FET: 2SK3608-01S (Datasheet is attached)
・Diode: RF081M2STR (Datasheet is attached)
・Transformer: custom
・Any protection function are not detect
・High temperature is only UC2825.
Board, FET, and the other components are not high temperature.
If there need detailed information, please let me know e-mail.
Best regards,
Satoshi