This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: BOOST_SEL_IRAMP calculation

Part Number: LP8860-Q1

Hi,

using the LP8860-Q1, I want to set the I_RAMP in EEPROM Address 0x71[6:3] – BOOST_SEL_IND, BOOST_SEL_IRAMP register. According to the App report http://www.ti.com/lit/an/snva789/snva789.pdf  equation (1) I get  a negative result for:

L=100µH

Vin_min=7V

Vout_max=32V

I_RAMP_GAIN=-5.352

What is wrong?

Thank you

Christian