This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM53601-Q1: Minimum Dmax value to perform WCCA

Part Number: LM53601-Q1

Hello,

I am working in calculating WCCA. I am looking for minimum Dmax value.

Please advise,

Thanks,

Arun C S S

  • Hello Arun,

    You can calculate the maximum duty factor while maintaining frequency using this device’s minimum off-time. Minimum off time is listed in the datasheet and has a maximum 125 ns. At 2.1 MHz, this gives a worst case maximum duty factor of 73.7%. If a higher duty factor is needed to regulate, frequency is automatically reduced.

    Regards, Robert