Hello
Currently, customers are applying circuit design with BQ24297.
condition
1. When a USB D +, D- line cable is connected to the product, the product recognizes it as USB and current limit is 500mA.
2. When connecting only the power cable without USB D + and D- line, the current is limited to 500mA while recognizing the product as USB.
3. When connected to Fast Charger adapter, it recognizes as adapter and confirm that it is charging without limitation to 2A.
Can I change the current limit when connecting a power cable with no USB D + or D-line in # 2?