This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5119: HICCUP mode

Part Number: LM5119


Hi

I'm testing a dual BUCK(13V,18V) by LM5119.

There is no problem with 13v but 18v start a hiccup at no load.
Looking at the data sheet, there seems to be only an over current related to the hiccup.
Can you be a hiccup for another reason?

-test condition

2-ch Buck(LM5119)

  1. Input: DC 66~100V

    Output: DC 13V / DC 18V

            DC 18V 1A(typ) / 11A(peak)