This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS24750: constant current limit feature

Guru 29720 points
Part Number: TPS24750
Other Parts Discussed in Thread: TPS2662, TPS2596

Hi Team,

My customer wants to limit output current at 100mA when load current increases more than 100mA.
He wants not to set fault timer, it is required that 100mA is continue to flow forever until output current decreases below 100mA.

Is the feature possible for TPS24750?
If the answer is no, I would like to know if there is TI device that meets the requirement.
Input voltage is 9V in this case.

Best Regards,
Yaita