This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25088: The MOSFET is very hot when the output is below -11V@2A

Part Number: LM25088

Hi 

  We design a negative circuit using LM25088. The spec is Vin=24V, Vout= -10 to -18V @1.5A. 

 When the output is below -11V(-11V, -12V, -15V, -18V)  with no load, the MOSFET AO4354 is very hot. the temperature is above 80℃. when it is on 1.5A load at with any VOUT, the temperature of  MOSFET rise up 110 ℃ quickly. We disable it.

Can you check the schematic to improve it ?