This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25145: 25145

Part Number: LM25145
Other Parts Discussed in Thread: LM5143-Q1

Hi,

I am using this controller LM25145 for my design.  My input voltage is 12V and output is 5.2V with 30A load current. 

This IC has current limitation of 20A . So someone here recommended me to use 2 phase for that much load current.

Can someone here guide me with that how do I achieve that as I have no idea of 2 phase thing.

Thank you