Other Parts Discussed in Thread: TPS92691,
Hi Sir
our customer want to use TPS92641 or TPS92691 to design as input:80-130V; output constant current 20A,Voltage=60V;output power is 1200W,the input voltage customer will use other external circuit to design meet the TPS92641 or TPS92691 input range,the drive circuit will add the gate drive NCP51530 ; pls help check the TPS92641 or TPS92691 can finish this design requirements?tks!