Other Parts Discussed in Thread: TPS62743, TPS62808
Hi team,
My customer is evaluating TPS82740ASIPR in a smart band project. But the 1.1 mm max height is still too high. So do we have any other solution that is within 0.8mm height? The other requirement is as below:
The input is 3.3V~4.2V.
The output is 3.3V/1mA and 1.9V/1mA.
The package can be different with TPS82740ASIPR but the length and width cannot be larger.
Thanks.
Best regards,
Wayne