This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: Compatibility of a 4.15 OCV solar panel

Part Number: BQ25504
Other Parts Discussed in Thread: BQ25505

Hi All,

I was just wondering whether using a 4.15 OCV solar panel for BQ25504 chip would cause any issues?.

Even though datasheet mentions an absolute maximum of 5.5V on the VIN_DC pin, can the chip still be be able to operate with MPPT at 3.35V of the solar panel.

The datasheet of the solar panel is as follows. It would be really great if I could know an answer ASAP.

Regards,

Sanchitha.