Hi,
I have two questions about STATUS pin under DCP_AUTO mode.
- When CTL1/2/3/ILIM_SEL is configured as "0011" (DCP_AUTO/Power WAKE LIMIT), if a current > IOS_PW (55mA typ) is detected, STATUS should be asserted low. Is there any debounce timing for STATUS to change from high to low at this moment? (For low-to-high scenario, there's a15 sec timing defined.)
- When CTL1/2/3/ILIM_SEL is configured as "0111" (DCP_AUTO/Non Power WAKE LIMIT), ILD is defined as a much higher threshold at 700mA/typ. May we know what kind of application scenario could need such setting? I didn't find an application example in the datasheet.
Thanks!
Antony