Hello,
There are some post relating this topic but I am still not sure our usage is possible. Please let me ask this.
1. What is made limit?
Figure 4, D package duty vs current graph
This limit will come from power dissipation. Do I think correctly?
2. Duty estimation
We use 6 of 7 channels. 6 channels split by 2 group, group 1 and group 2. Each group has 3 channels. Each group requires the same current like 100mA each.
There are four status.
1) Group 1 current flow, Group 2 doesn't flow -> called this 1
2) Group 1 current flow, Group 2 flow -> called this 2 (= 1+1)
3) Group 1 doesn't flow, Group 2 flow -> called this 1
4) Group 1 doesn't flow, Group 2 doesn't flow -> called this 0
1,1,2,1,1,0,0,0 is repeated. I assumed this duty cycle 75% (= 6 / 8). Is this estimation right?
3. Total drive ability
Assumed this 75% duty, I can see each channel can flow around 95mA from figure 4. We combine 3 channels so total around 285mA load can drive.
Is my estimation correct?
I think ULN2003A can drive around 285mA load when ambient temperature is 70C. Would you review if I can consider correctly?
Best regards,
Toshihiro Watanabe