Other Parts Discussed in Thread: LM5069, TPS24720
Hello Sir,
1.) I am using LM9061-Q1 high side gate driver in one of my applications. I have done a calculation for worst case scenario and I am switching a mosfet with this high side driver.
I am having a maximum drain to source voltage drop of 40 millivolts, after which the protection comparator will get activated and the driver has to be in latch off mode.
For this application, I have taken Rthreshold = 560 ohms and Rsense = 500 ohms. Is these values will be okay for making the gate driver to latch off ?
Also is it necessary to use Rsense resistor?
2.) Do i need to provide any overtemperature protection for the mosfet?
Because anyways the driver will protect it from overcurrent protection.