Other Parts Discussed in Thread: BQ78350
Hi,
I have a question about BQ78350-R1 with FW 2.02 installed.
I want to disable both CHG and DSG FETs usign an external logic circuit. I can use both SMBUS or discrete signal to do it and I want to do it when BMS is in sealed mode.
I see that PRES pin can disable both FETs. Can I use this pin to disable or enable FETs even if the battery pack remains connected to BMS? Can I power-on BMS from shutdown or sleep with the PRES pin high (FET disabled)? Can I shutdown BMS with PRES pin high (FET disabled)?
Thanks in advance