Other Parts Discussed in Thread: TLC555
Dear Sir/Ms.
Our customer currently design the TLC5955RTQR as a stack of 5 strings.
The test found the following problems.
1. The temperature of the first one will be higher than the latter. Will this be the case with actual use?
2. The last TLC5955 is not full, but the last TLC555 channel is broken down (low impedance). Have you seen this situation? How to design the channel that is not used?
3. Throw into the ring temperature furnace. When the IC temperature is greater than 85 degrees C, abnormal operation will occur (for example: the current of each channel cannot be turned off, and the output is always 20mA). The restart is also the same. The entire board must be taken out and cooled down before it will return to normal again. Is this situation normal?
4. If the LED Vf=3V, what is the VLED voltage I need?
At present, the channel needs to be set to 20mA due to the demand. The actual VLED=6V~~ is designed. Is there any problem with the design? How to calculate the peripheral circuit?
This customer is very good. If you still want more information to judge, please let me know, I can ask the customer.
Best Regards,
Kami Huang