Other Parts Discussed in Thread: BQ24610,
Dear Sir, good morning
I have 5.1 V power supply - conventional power supply, is not a solar panel.
Please, answer:
1) Can I charge 1-cell lead-aсid battery? ( "bulk voltage" = 2,47 V; "float voltage" = 2,35 V). Battery charge will occur in the temperature range from minus 40 to pluis 60 C.
2) Can I set 3A charge current during CC charging? (as I have 25AH 2V cell and I would like to charge it quickly).
3) I see, that circuit on the figure 2 has two outputs: System Load and Battery Pack. Can I connect load to Battery Pack out? If connect the load to System Load out, then the voltage on it will be less by the amount of the drop on the diode D3.
4) What voltage I need to feed to TS input?
TIA
Sincerely,
Vladimir Naumenkov
www.agat.by application note bq24650.pdf