Hello,
It has 5V MCU implemenation for TPS2H000 in the datasheet, but needs reference schematic for 3.3V MCU.
What is the recommended value for R(pullup), R(ser) and R(cs) for 3.3V MCU?
Because Vcs(h) can be 4.5~6.5V, it would need voltage divider to connect CS pin to 3.3V ADC input.
Is there're any recommended resistance for the divider?
Iout normal is 250mA and current limit is 0.5A as design requirement.
Thank you in advance.