An old project of our company use UCC27324
Does UCC27324 have new version?
or another better version?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
An old project of our company use UCC27324
Does UCC27324 have new version?
or another better version?
Hi Gary,
Thanks for reaching out to the High Power Drivers team, my name is Mamadou Diallo, I am the AE supporting low-side drivers.
Please see attached few drivers that are pin-2-pin and drop-in upgrade over UCC27324 in switching characteristics. These devices use enable pins (pin 1 and pin 8) that are internally pulled HIGH to VDD level. This makes the devices p2p with the UCC27324.
UCC27324 | UCC27524 | UCC27524A | |
Datasheet | Datasheet | Datasheet | |
Number of channels (# ) | 2 | 2 | 2 |
Power switch | MOSFET | MOSFET | MOSFET |
IGBT | IGBT | ||
GaNFET | GaNFET | ||
Peak output current (A ) | 4 | 5 | 5 |
Input VCC (Min ) (V ) | 4.5 | 4.5 | 4.5 |
Input VCC (Max ) (V ) | 15 | 18 | 18 |
Rise time (ns ) | 20 | 7 | 7 |
Fall time (ns ) | 15 | 6 | 6 |
Input threshold | CMOS | CMOS | CMOS |
TTL | TTL | TTL | |
Prop delay (ns ) | 25 | 13 | 13 |
Features | Dual Non-inverting Outputs | Enable Pin | Enable Pin |
Hysteretic Logic | |||
Operating temperature range (C ) | -40 to 125 | -40 to 140 | -40 to 140 |
Package Group | MSOP-PowerPAD | 8 | MSOP-PowerPAD | 8 | MSOP-PowerPAD | 8 |
PDIP | 8 | PDIP | 8 | SOIC | 8 | |
SOIC | 8 | SOIC | 8 | ||
SON | 8 |
Please let us know if you have further questions or press the green button if this addressed your questions.
Regards,
-Mamadou