This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3836: Can we connect CT pin to GND with a capacitor to modify the delay time?

Part Number: TPS3836


Hi,

As the title, Can we connect CT pin to GND with a capacitor to modify the delay time as 20m Sec?

Or is there any method to modify the delay time?

Thank you.

  • Hi user,

    You should only connect the CT pin to GND without a capacitor to achieve a 10ms delay for the TPS3836. This is not an adjustable delay part and is also not open-drain, which means it won't be able to achieve 20ms delay and we also can't rig up external delay with a capacitor/buffer solution.

    That being said, we have many supervisors in our portfolio that can achieve 20ms delay, you should check out our quick reference guide to see what fits your solution the best.

    Thanks,
    Abhinav.