Hi,
My system is having BQ25892 part. Even though Charging settings looks ok, I don't see Battery voltage increasing.
When I connect power meter, I see current flowing into system is around 1.4A only even though Charger can supply 3A. Not suspecting Charger since I see same charger able to pump 2.8A - 2.9A on other system with different Charger IC.
Charger used - TypeC NonPD Choetech 5v/3A charger.
Battery voltage - 3.8 (Max. 4.4V)
Charger IC dump:
0x4 0x3F
0x6 0x7E
0x0 0x1C
0x3 0x1A
0xB 0x16
Thanks.