Tool/software: WEBENCH® Design Tools
Hello. I am designing a power supply circuit with an operating voltage range of 18-65 volts and a current limit of 7 amperes on the LM5088-1 microcircuit. I assembled a printed circuit board. It works stably, protection against short circuit on the output works. But, for some reason, the chip fails when the input voltage rises above 45 volts and makes a short circuit at the output. Burns without noise and smoke. just lost generation on the gate. Burned 3 chips. I can not understand where the error was, did everything as suggested by the designer. The transistor took IRF3710 choke srp1265a-330m at 33 uh and 8 amps. Who can tell what the error is?