This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm having buzzing noise with the "AN-2102 LM3464 and LM5021 DHC 25W EVM" that I bought from TI. Any idea why?
The issue gets worse when using a triac dimmer. Can we use a triac dimmer with this board inserted in series with the L line?
Thanks
Sana
Hello Sana,
Where does this state it can be used with a triac dimmer? That requires different circuitry and control signals to adjust light output. It is a much more difficult design to be compatible with a triac dimmer and also control the secondary side current output. A better approach would be not to use a DHC regulator for the first stage, a voltage regulation PFC would be better. Then a secondary stage that consists of buck converters. A DHC may not reject variances in a triac dimmer function causing light fluctuation. A triac decoder would be needed to set the buck converter output power/current. The LM3450 data sheet has information on this though it may not be exactly what you are looking to do. There are also circuits with the UCC28810/11 that are two stage designs.
Are you stating there is a buzzing noise when connected direct to AC (no dimmer in the circuit)? Buzzing is a common issue when triac dimming, this was not intended to be triac dimmed.
Best Regards,
Hello Irwin,
Thank you for taking the time to respond.
The buzzing is existing with and w/o the trial dimmer at the input AC line. It is worse and very noticeable though with the triac dimmer.
Is it normal to have buzzing w/o triac dimmer?
Thank you.
Sana Rezgui
"The LM5021 EVM was not intended for triac dimming, the LM3464A EVM was not intended for triac dimming either. There are other designs that exist specifically for triac dimming. Designing for triac dimming requires a different design approach."
Understood.
"Can the LM3464A interface to a current source that is triac dimmed? Probably, however it probably doesn't make sense to do a design this way."
Understood.
"You have to locate the noise. I would assume it's 60/120 Hz noise however it can be something else. Solving this is just trying to find the offending parts, changing them, mounting them to the PCB different or possibly pot/RTV the component."
As I said, I believe the noise is coming from the transformer. I was hoping that the demo board would reflect a reference design with no issues.
I have already filed another case for the second 3464A EVM (w/o the LM5021) board. You will see it probably soon.
Thanks.
Sana
Hi Irwin,
The buzzing is really substantial, when I use the PWM dimmer as well. A demo board should reflect a typical well operating condition.
I'm glad that I know about the issue now. I'll try vacuuming but I don't think that it will solve such noise.
Thank you through for trying to help.
Sana