Other Parts Discussed in Thread: OPA552, , TPS61175, TPS55340
Hi, I'm using +-30V high voltage OPA552 Op Amp from TI. I have used this Op Amp with an external power supply until now.
However, I have to make this as a battery powered product with CC3320 Wi-Fi chip.
I'm using a Lithium Ion Polymer Battery - 3.7v 500mAh.
https://www.adafruit.com/product/1578
The only idea I had was to use a boost converter and enable the boost converter's output for a short time to save the battery life.
Later, I will be changing the Op Amp to another one that supports more higher voltage.
These are my questions;
Q0. I cannot find TPS61390 from Digikey or Mouser. Since this is a new product, can't I buy this online now?
Q1. For now, I have to generate +30V and -30V with the TPS61390.
Just like this connection, is it possible to create +30V and -30V with two TPS61390?
Q2. To extend the battery life, I will toggle the EN (Enable pin) really shortly.
How fast am I allowed to toggle the EN pin? I just need to enable the boost converter for 1μs so I hope the EN pin can detect this sudden change.
Or I'm worried whether the boost converter needs more time to turn on.
Q3. Lastly, for battery-powered applications, is using two boost converter to power the Op Amp a good idea?
My desired power supply is +70V -70V so this output surely meets my desire.
However, the boost converter draws many currents so I'm curious whether there is a better way.
Thanks for your help.