This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063A: About Charging Current to Timing Capacitor

Part Number: MC34063A


Dear Sir or Madam,

When deciding on a timing capacitor, the following questions should be addressed, so please give me good advice.

The following formula which described in
the Application Report: SLVA252B
Chapter 3.4 Timing Capacitor Calculation

the formula:
Ct = Ichg (min) * (Δt / ΔV)
     = 20 x 10-6 * (ton / 0.5)
     = 4.0 × 10-5 * (ton)

it has become "Ichg (min) = 20 uA".

However, Ichg specifications have become
24uA (min), 35uA (typ), 42uA (max)
on MC34063A data sheet: SLLS636N.

The value of Ichg(mini) is different between the two.
How should I think about "Ichg (min): 20uA" in the equation for Ct?

Sincerely yours,
Hirofumi Sekido