Hi Experts,
There is an item to set the OFF delay time of synchronous rectification on page 19 of the data sheet. On page 53, there is a comment that "A good place to set these delays is 50% of tABSET.". While a dead-time between A and B is decreasing when a load is increasing, a OFF delay between E and F is increasing when a load is increasing.
Is there any recommended % of load when we should set them as 50%?
If a delay between E and F is larger than a dead-time between A and B, are there any chance that a surge or anything occurs?
Regards,
Uchikoshi