This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: eFuse IEC60950-1 and IEC62368-1 compliance

Part Number: TPS1663
Other Parts Discussed in Thread: TPS2663

Hi,

I have a question about your eFuses, and the TPS1663 in particular.  

Is it possible to use this to design a limited power supply that complies with 2.5 in IEC60950-1? And to claim an energy source classification that complies with 5.2 in IEC62368-1?

Does the component  complies with the single fault conditions that are described in these two standards?

Br

Fredrik