This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08T240W: The output of PTH08T240W is 0 V

Part Number: PTH08T240W

Hi:

          The normal output of PTH08T240W is 1.2V, but due to the short circuit of 10uF load capacitor at the output end, after replacing the new load capacitor, PTH08T240W can output 1.2V normally. But after a period of operation, the output becomes 0V. I see PTH08T240W has the function of current protection. I wonder if the short circuit of load capacitor will damage the function of PTH08T240W. Is there any good solution? Thank you very much.