This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426: definition of "temperature and load compensation"

Part Number: BQ27426

Hi there,

most of the metrics are available from the chip under 3 forms: Raw, Compensated, Filtered... 

When they are labeleld "compensated for load and temperature", is it using an "instantaneous" current measurement? Or is it am average which represents a typical use case of the application?

For example:

- If I have a current spike of 200mA for 100ms, but my average current consumption is 15mA (which the chip can average across multitple battery cycles) - which one is used by the compensation algorithm?  

Thanks for your help,

Mickael