Hi
I have a question about dropout mode of LM317.
If Vin belowed Vout, does Vout track Vin or become 0V?
Best regards,
Yokota
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Hi Yokota,
I believe that the condition you are asking about is if Vin is less than the set output voltage for LM317 (Vout_nom). If this is incorrect, please let me know.
In order to ensure a regulated output voltage, Vin should be equal to Vout_nom plus 3 V. If Vin is less than Vout_nom plus 3 V, the output may drop out of regulation in which case it would track Vin as you described.
Very Respectfully,
Ryan