This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: reference circuit for 5V input, 56V/0.6A output at 60 degree C, non-isolation

Part Number: LM5122


Hi Sir,

My customer is looking for a reference design for  5V input, 56V/0.6A output at 60 degree C, non-isolation.

I try to use webench to run with LM5122, it could only run at 30 degreeC, but at 60 degreeC, it will show not able to support.

Could you help me to check if this is simulation issue or this is a limitation of LM5122?

And if LM5122 could not support above requirement, what other IC you suggest?

We also need your help to provide the circuit if possible.

Many thanks.

Patrick