This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: The relationship between the length of the sampling line and the accuracy

Part Number: BQ79606A-Q1

hello

In the BMS project, we found that when the sampling line is 2 meters, the voltage of the two sections of the cell is the same as that of the test panel. When the sampling line is 0.2 meters, the voltage of the two sections of the cell is 6mv higher than that of the test panel.How should the compensation be set according to the length of the sampling line?