This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV733P-Q1: higher PSRR solution

Part Number: TLV733P-Q1
Other Parts Discussed in Thread: LP5907-Q1, TLV702-Q1, , LP5912-Q1, LP5912

Hi Sir,

My customer is using TLV73333PQDRVRQ1/TLV73318PQDRVRQ1 on their system, and facing a PSRR issue.

So they are looking for a higher PSRR solution with same package and pin out.

The requirement as below:

LDO 5V to 3.3V, LDO 5V to 1.8V.

Iout: >300mA

High PSRR, (> 65dB(min)@1KHz~3KHz ; >55 dB(min)@3KHz~30KHz)

Many thanks,

Patrick