Hi,
For our new design, we have to use 12 V power supply and 3.7V battery as power input.
Battery operation is only for 30 minutes if power fails.
My maximum current requirement is 50 Watts.
My requirements are below.
1A max at 12V rai
5A max at 5V rail.
3.5A max at 3.3V rail.
200 mA max at 1.5V rail.
I need to use a single cell Li-Ion battery charger also in my circuit.
Can you suggest a possible power tree with available regulators and battery charger from TI.
Note: My battery cut-off voltage is 3V.
And all above mentioned voltage should be available if main power (12V) fails (at battery operated time).
Best Regards,
Shafeeq