Other Parts Discussed in Thread: LM2621, TPS61022, TPS61089, LM2662
I want to boost from Vin=approx.1V to Vout=12V. Iout should be 200mA.
The input voltage should be as low as possible because the source will be a 2.5V supercap. So at the beginning Vin will be 2.5V and decreasing constantly. However the boost circuity should switch off at a very low Vin in order to get the maximum out of supercapacitor's charge.
Will a LM2621 or LM2623 be suitable, or which other step-up converter do you suggest?
Thank you.