This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072T: Problem with calculating the termistor values

Part Number: BQ24072T


Hi,

I want the BQ24072T to charge between 5°C and 40°C.

According to the sensor datasheet, R_Cold is 22.02kOhm and R_Hot is 5.827kOhm. I have calculated the following values:

R6: 31,7k (Used value is 31.6k)

R7: 20.3k

R8=100k

But when I use these values and adjust the resistance of the termistor (using a potentiometer), the charging will not stop until approximatery 30kOhm which is below 0°C according to the sensor datasheet.

(103AT, Beta=3435K, R25=10kOhm)

Are my calculated values wrong?

Thanks