Other Parts Discussed in Thread: LM5155, TPS40210
it is possible to connect ISEN- pin to gnd, and ISEN+ pin to sense resistor in mosfet source path?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear sir,
The sensed signal from the input line is more clean than from the low side FET. If from the low side FET, there need to add addtional filters. So suggest you keep the sense resistor in series with the inductors.
The expert for this part is on US holiday and they'll reply you after back to the office.
I have very wide input voltage range from 15V to 400V and discontinuous conduction mode boost. I need a minimum duty cycle of 1% and i can't do that with frequency higher than 50kHz.. Also i need adaptive soft start with duration of few second.
Can you recommend some controller for this application?
With TPS40210 is hard to get adaptive SS, LM5155 is perfect but duty cycle is greater than 1%...