Other Parts Discussed in Thread: TL432, TLV431
Dear Team,
I'm using TPS23751 in my design. The design is similar like PMP111254.
Everything is fine until the secondary load reaches 6W. Whet it reach the 6W, the controller VDD and VSS pin goes to short circuit, and sometimes brings the primary FET to die.
I reviewd the schematic many times, I found some problem on it(I used TLV431 instead of TL432, and the soft start capacitor was in a wrong position). After I corrected these issues, the result is the same.
I temporary attached a 750k feed forward resistor, but it not resolved the issue.
I tryed WE 7491195112 instead of Colicraft POE300F-12L, but it not resolved the issue.
You can find the schematic below.
If you have any idea please let me know.